Hello,
I've been trying out some different types of amplifiers for my application where I need to amplify a differential signal. Originally, I tried an instrumentation amp, but this proved to be too bulky with resistors and all for setting gains (I need to use a TSSOP package size with 2 circuits). Size is one of the biggest constraints because I will be soldering in free space, not on a circuit board. I next tried THS4522 which is low-power differential amp. I'm not too concerned about low-power, but I don't want dual output. I'm looking for a chip that has 2 circuits, each of which take the difference of two inputs and provide only one output. My preference is a fixed gain amplifier, that doesn't necessarily have to be that big (it could even be unity gain). Any help selecting an appropriate chip would be greatly appreciated.
Kyle