Hello,
I am looking for an alternative to the OPA140 with an increased Common-Mode Voltage Range? My application is similar to the one in figure 3 of http://e2e.ti.com/blogs_/b/thesignal/archive/2012/03/21/differential-input-clamps-can-they-affect-your-op-amp-circuits.aspx
Due to the high slew rates in such an application, I would prefere to use an op amp without clamp diodes in the op amp input.
My supply voltage is +-12V, and according to the data sheet of the OPA 140, the upper limit of the Common-Mode Voltage Range is (V+)–3.5. The input signal range of my application is +-10V. Therefore, I am looking for an alternative to the OPA140 with a higher Common-Voltage Range.
Further more, the application requires unity-gain stability, slew rate > =10V/µs and output current >=4mA.
Regards,
Steffen