This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can plastic package op amps be IR re-flow soldered? If so, does TI publish a safe re-flow curve? I've seen many papers in the TI library on methods, techniques, tools etc., but can not find a recommended safe curve, assuming that it's the same for all P-DIP and P-SOIC packages. Even a chart on the maximum time vs. temperature exposure would be helpful.
Do you have a particular part in mind? I've included a link that covers some of our parts.
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=SNOA549
Hi Loren
I'm a little confused by the chart as it seems that as the package gets thicker and larger by volume it's ability to withstand prolonged heat diminishes. To me this is counter intuitive. We use many TI and BB parts in our designs and we also prototype and redesign with many others. Here is a partial list of the most popular:
TLE2071
THS3061 3091
OPA1611 627 827 211 1641 134
INA163 134
LME49710 49713, 49870
In some above we also use their dual versions.
All above are SOIC 8 (except INA163 SO-14) for the most part, some are DIP 8 but we can continue hand soldering those.
We use either the lead or lead free (whichever is available through distributors.)
The solder requires a maximum tempereature of 246C for only 4 seconds, but is above 240C for a total of 12 seconds.
It would be convenient if TI had a chart that, at the very least, listed all packages by their thickness and volume, and desirable if the white papers listed the the max temperature and time for each device. The best would be a graph of maximum temp and time as Vishay shows for their Z-foil resistors.