This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Opamp as a Buffer for driving high capacitive load ( appx. 100nF & 10 Ohm resistor)

Other Parts Discussed in Thread: THS4271, LM8261, TINA-TI, LM7322, LM8272, LM7121, LM8262, LM7321

Hi,

Could someone please suggest a suitable opamp which can be used as a unit gain (buffer) configuration?.

This opamp should be able to drive a load with capacitance of 100nF(Appx.) & 10 Ohm resistance;

the O/P current sourcing capability should be >200 mA and Bandwidth of atleast 50MHz.

I was looking at THS4271 but could not find anything related to its capability of driving Capacitive load.

Please let me know your thoughts/inputs.

Regards

Bijeta C