Hello,
I was wondering if this particular Op-Amp(LM8262) outputted a constant current of 60mA. I'm using this as a voltage follower. I have noticed that some Op-amps will output different current values when setup in this manner while having the same output voltage. So if I were to put this Op-amp in my circuit would I have and output current of 60mA with the same Voltage I'm having with all other op-amps?
I'm outputting a voltage of 2.5V with a current of 30mA, if I use this op-amp would I have a voltage of 2.5 V with a current of 60mA?
Thanks,
-Sahil