hello,
I am going to drive TLV4112 by TPS780300250DRV, set to 2.5V output.
will TLV4112 work safe at 2.5V power supply, does it need any margin at the low side of the specification.
thanks,
David Sun
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,
I am going to drive TLV4112 by TPS780300250DRV, set to 2.5V output.
will TLV4112 work safe at 2.5V power supply, does it need any margin at the low side of the specification.
thanks,
David Sun
Hello David,
The minimum supply voltage rating for the TLV4112 is 2.5 V so it will be operational with that supply level. As long as the voltage doesn't drop below this minimum it should be okay.
Do note that the amplifier's common-mode input voltage range VICR is not from supply rail to supply rail, but instead from 0 V to VDD - 1.5 V. Thus, the VICR is 0 V to 1.0 V with a 2.5 V supply.
The output voltage swings close to the supply rails; especially at very low output current levels. The TLV4112 Electrical Characteristics tables lists it to be within 300 mV of the positive rail, and 100 mV of the negative rail (IO = 10 mA), for the 3 V and 5 V supply conditions. The swing levels should be about the same for a 2.5 V supply.
Regards, Thomas
PA - Linear Applications Engineering