This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
I just tumbled over a bunch of application note, which where really helpfull but didn't really answered my question. Here it comes:
I have an audio codec which outputs a differential analog signal with an offset of 2.5V so that the signal is between 0.875V and 4.125V on both outputs. Now I'd like to use a differential amplifier as a line driver. By using standard OPAs I wouldn't need any negative voltage supply. How about differential amplifiers? Is there a way or is this a waste of time to think about? The application note "Differential Op Amp Single-Supply Design Techniques" explains how to use a FDA with only one supply but with a single ended input. I guess this doesn't work with a differential input?
Thanks for your help!
Regards,
Lennart