Other Parts Discussed in Thread: THS4500, THS4130, THS4521
Hello, I'm using a FDA to reject a 2.5V offset of my signal and amplify the signal such that when it goes through a peak detector, it'll be at 5V.
When using dual supply, I am able easily achieve this.
However, when changing the configuration to a single supply, the signal will clip if I try to make it 5V.
I display my schematic and plots in the file.
I was wondering if there was a way to solve this?
On a side note, the PD pin of THS4521 says the max is 2.1V but I'm only allowed to use 2.5 and 5V power supplies. I was wondering If I can shove 2.5V down the PD pin like I did in the simulation.