This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
INA199A1 What is the difference with INA199B1 function ?
Hello James,
The differnce between A and B devices is that B devices have a different ESD structures that are not susceptible to latching with large and fast transient signals (>2kV per microsecond) at the device input pins. So B devices are better suited for those applications where such large and fast transient signals may be present.