This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer Goodtime is using 555 timer in their e-horn product, they are evaluating both SA555 and TLC555, would you please help to provide the ESD protection spec of both device? And is there any difference between TTL and LinCMOS in ESD protection? thanks.
Kevin
Hi Kevin,
The only Qualification Report I could locate for the TLC555 is one for the automotive version, but the ESD performance should be the same. The ESD results for it are:
HBM 1 kV
MM 200 V
CDM 2 kV
Regards, Thomas
PA - Linear Applications Engineering