This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Padmaja,
I support the BUF634 for Precision Analog. We don't offer a multi-channel version of the product. Although I am not directly associated with the video multiplexer products, could you consider using a 4:1 video multiplexer such as the LMH6574? It has a buffered output capable of providing up to +/-80 mA.
http://www.ti.com/lit/ds/symlink/lmh6574.pdf
Regards, Thomas
PA - Linear Applications Engineering
Hi Padmaja,
The LM6574 should handle your 3 Vpp (+/-1.5 Vp) input signal if a +/-5 V supply is used. The no-load output can be as high as +/-3.53 V minimum, and the 100-Ohm load output can be as high +/-3.17 V minimum, both across temperature. The common-mode input range (CMIR) is rated at +/-2.5 V which is fine for the +/-1.5 Vp input. You can set the gain as needed providing you don't violate the output swing range of the amplifier.
Please note that the LM6574 is supported by TI's High-Speed Amplifiers group. They have an E2E forum and should be able to provide more detailed information about the product than I am able to from the Precision Amplifiers product forum. Here is link to their forum should you need it:
Regards, Thomas
PA - Linear Applications Engineering