I recently purchased the SensorEmulatorEVM Evaluation Module.
I also have the
PGA309 Test Board and USB DAQ Platform set
(2) PGA reference designs PCBA;s constructed.
I'm wishing to set-up the SensorEmulatorEVM to do "what-if's" and aid in the selection of my pressure sensor strain gauge.
The problem that I am having is that the documentation supplied CD with the SensorEmulatorEVM Evaluation Module is showing older "dated" accessories hooked up to the SensorEmulatorEVM Evaluation Module.
On the supplied CD of the (2) PGA reference designs PCBA;s constructed the docs PGA309 Quick Start_sboa103c.pdf and PGA309 Quick Start_sboa103c.pdf are not referring to the PGA309 Test Board and USB DAQ Platform set.
I presume the older "PGA309 Sensor Interface Board" is equivalent to the "PGA309 Test Board" which I have therefore I can substitute the PGA309 Test Board or one of my (2) PGA reference designs PCBA;s I have constructed as well?
The instructions as such are not clear to me on hooking up as they are referring to other accessories which I presume were offered in the past.
The Sensor Emulator I won't need to use for temperature simulation, I have my design setup for using the temp sensor internal to the PGA309 so I really just need the Sensor Emulator to provide a zero and span output and then vary it around for my "what-ifs'. So it's not clear to me if I can just use this for the bridge simulation without hooking up the temperature terminals or worrying about the Sensor Emulator jumper settings?
So if there is any documentation updated for using the Sensor Emulator with the latest PGA309 Test Board and USB DAQ Platform set please advise.
I also plan on using the PGA309 Test Board and USB DAQ Platform set with the (2) PGA reference designs PCBA;s I have constructed as well.