This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to measure a high accurate current range from 4mA to 20 mA by using Arduino Uno which has ADC 10 bits. Is RCV420 precise enough to get the exact current value from my Arduino.
I appreciate any help
Hi Collin,
I have bought the IC and I want to test .... First, I want to protect it from current above 20mA shall I follow this instructions :
www.ti.com/.../sbva003.pdf
Second, I want to test it but the power supply I have has a minimum 100mA ..... I want to use a current divider to down the current to 1mA
is that possible and how to design the current divider ??
I will appreciate any help
Best regards,
Hello,
The circuit you referenced provides an effective way to prevent damage from high current flow through the RCV420. I'm not sure what you mean about your power supply. It sounds like you have a 100mA current limit on your power supply, try connecting the power-supply to the RCV420 and see what happens. I don't think you'll need a current divider as suggested.