Other Parts Discussed in Thread: LMH2110
Hello,
I have question about LMH2110.
Q1:
Our customer would like to measure the traveling wave and the reflected wave,that they using two LMH2110.
They considering the attached circuit.
Could you please check attached file?
Q2:
RF frequency range of LMH2110 is 50MHz to 8GHz,it wrote in datasheet.
However,Figure 7's data is wrote from 10MHz.
They would like to input RF frequency at 46.35MHz.
In this case, can it take property?
Best regards,
Manabu ItoLMH2110 circuit.pptx