This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Hello Sehwan,
Analog and mixed-signal circuits can be susceptible to electromagnetic interference (EMI) generated by other electronic devices. If the switching power supply, or a switching supply inside the lamp, are dirty and producing a wide spectrum of RF signals they can be radiated from the circuits themselves, via the power cords and/or other cables connected to the devices. I suspect that if you physically move your circuit away from the EMI sources the noise decreases which would indicates that the EMI is getting to your circuit as radiated RF energy.
You have added some series RC networks at the input and output of the OPA2373, but that doesn't necessarily mean that they provide the optimal solution for eliminating your circuit's susceptibility to EMI. Radiated EMI could require one, or more, remedies to eliminate the circuit's susceptibility to the EMI such as input filtering, correct power supply decoupling at the IC pins, a correct PC board layout that eliminates the antennas that receive the EMI and couple it to the ICs, shielding, etc. You have mentioned how you constructed the circuit and it may be that you haven't taken any steps to prevent EMI from affecting your circuit.
There is a wealth of information about EMI and electromagnetic comparability (EMC) on line. A good place to start learning about the subject is the Henry Ott Consultants webpage. In particular see the Tech Tips and Technical Articles/Talks. A number of us here at this TI location have attended his sessions and use his book, Electromagnetic Comparability Engineering, as a reference when troubleshooting EMI issues. In my opinion he provides practical, sound advice on the subject.
Regards, Thomas
PA - Linear Applications Engineering