This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a device that has 4-20mA output, referenced to circuit ground, which I used XTR111 to realize the transmitter. This device works without problem in most situations. But I got reports that in some situations, it has some issues. When the receiver(a plc) is connected to the transmitter over 30-40m shielded cable (grounded on the receiver side) in an industrial environment the output increases suddenly about 1-1.5mA at the receiver side and oscillates a bit.. I did not inspect the site yet but they say plc has a 220V supply which is a EH150 Hitachi plc. Also they say when the connection to the plc is severed the situation goes away. They also say, there is no voltage or anything at plc analog input. I've tried with 100m cable with different type of receivers with seperated ground with the transmitter in the office and did not face any problem. What may be the issue? Does using current loop transmitter like xtr117 may improve the situation? May isolating the mA improves the issue? Thanks.
Hello Mustafa,
4-20mA loop drivers are intended to communicate over extremely long distances and the 30-40m of cabling is not uncommon, so while I'm not immediately sure what's going on in their system I have a few suggestions.
It sounds like there may be something going on when the shield is connected to the GND on the receiver side of the system. Does the system behave normally when the shield is left floating or is grounded on both sides? What potential is the shield connected to relative to the GND on the XTR111?
Since they're using a shielded cable I'm guessing they operate in a noisy environment, is it possible that they're seeing some type of higher frequency energy in the system being rectified down to a dc offset? Both radiated and conducted emissions can cause dc shifts in the XTR output. If this is the case then 2-wire transmitter topologies (XTR115/67) are typically more immune to both conducted and radiated emissions.
I inspected the device that has an analog 4-20mA output that works without problem in the same environment and it has an isolated analog output but is not current loop. That device has 220VAC power supply input and analog output section has 10V isolated and regulated supply. The mA- output is same with the gnd of the 10V isolated supply. So it is not a current loop. The receiver side is also isolated but I don't exactly know it's input circuit (
Hi Mustafa,
Actually based on your description, the transmitter is definitely a 3 or 4-wire transmitter which is why your 2-wire transmitter circuitry doesn't work. 2-wire transmitters receive power from the loop and transmit the signal back in the form of a 4-20mA output. Therefore, 2-wire receivers provide the loop-supply to the transmitter and measure the current the transmitter returns. 4-wire receivers do not provide the loop-supply on the same wires as the output current so if you plug a 2-wire transmitter into a 4-wire receiver input channels then the 2-wire transmitter will not be powered. I suggest you go through the 2-wire and 4-wire blog posts that I previously referenced to gain a better understanding of how these systems look and how to connect to them.
Here's the 4-wire transmitter posts again for reference: