Other Parts Discussed in Thread: OPA454, THS6212
Hello,
I am looking for guidance for TI part numbers to help me with a project. I need to amplify a video signal down a 15 AWG shielded wire, approximately 5 KM. The video signal is a NTSC/PAL composite signal 1 volt P/P, 540 TVL, 768H x 576V. I have estimated the voltage drop along the line to be about 45 volts, so I would assume the signal would need to be boosted by ~50 volts to achieve this. Does anyone have any suggestions or any TI circuit diagrams you can send to lead me in the right direction? I was originally looking at the OPA454 high voltage OpAmp but noticed the slew rate was only rated around 13 volts/us. My signal runs over 100 volts/us slew rate I believe so this wouldn't work. Any help would be greatly appreciated. Thanks.