Hi all,
After using XTR110 for a new design we have some questions about it:
- We need an operating temperature range of -40-85ºC so we chose the ceramc AG version. Now this model is NRND and it is difficult to find it at our common providers (such as farnell, mouser, digikey...). Moreover we need to manufacture our product during years and we are afraid about product obsolescence, is there any way to solve this and keep using this IC the next years (not only buying the higher possible quantities from distributors now)?
- Another possible solution is to use the plastic package which is rated to 0-70ºC (though datasheet temperature shows specification and operating, this last one is -25-85ºC). So, what is the impact of exceeding this temperature during operation? I mean, exceeding temperature could cause destruction or just some temperature de-rating in some datasheet parameters? We can test this in a climatic chamber but we prefer to do this previous analysis.
Thanks in advance,
Regards.