In a application, the LM119 inputs were accidentally pulled as much as 30V below -Vcc pin. What is the maximum voltage that the inputs can be below -Vcc before the input transistor fuse short? I have reviewed the datasheet and understand that the Absolute max that the part is stressed when the input is below -Vcc. The question is how far can the input go before the input transistors are certain to fuse short?
I would like to discuss our situation with a subject matter expert to go over these details. Is that possible?