Hi,
LM7301, V+ = 3.1V, output is pulled up by 2.2k resistor to 5V. Any issue in long run?
Thanks.
- YY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
LM7301, V+ = 3.1V, output is pulled up by 2.2k resistor to 5V. Any issue in long run?
Thanks.
- YY
Hello Yee,
Will the LM7301 still have the 3.3V supply applied? Or are you thinking of a V+ power-down condition (V+ around 0V with output thru 2.2K to 5V)?.
Max current with the supply off would be 5V/2.2k= 2.3mA. That is a little higher than we generally recommend (<1mA), but below the 20mA Abs Max.
Note that this will affect the lower output swing (~200mV to rail) as the LM7301 will have to continuously sink 2.3mA (plus any load and feedback resistor current) when swinging low. The LM7301 will be biased into a class A mode and continuously sinking. The LM7301 is a low power amp, and the 2mA is using up about 20% of the available output drive.
It should not harm it, but I would place a Schottky clamp diode from the output to the V+ supply to shunt the current around the internal clamp diodes should the V+ supply drop with the 5V still applied.
Regards,