From my understanding, if the source pin is able to complete its edge transition before the signal reaches the load pin, then it is a good idea to control the routing impedance. With that being said, both output traces of the OPA1632 in my design are only 3inches long and the maximum frequency is 1kHz, maximum voltage is 1.5V. Would you recommend controlling the impedance or do you agree that in this case it is insignificant?