This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6401: LMH6401

Part Number: LMH6401

Hello,

I am using LMH 6401 in ac coupled configuration to amplify the AC signal which is then followed by a RF power detector to convert the same signal into DC. I am a little bit confused with PD and Vocm Pins since i pulled PD pin to low (connected to ground) and Vocm is also pulled to ground with 10nF capacitor. Is this right or did i make some mistake for these pins.

Regarding gain amplification which ca be done digitally , can i get some help in that regards.

Thanks and Regards