This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to confirm following information.
* Rθja, Ψjt and Ψjb
It seems that there is no information about thermal information in datasheet.
At least, could you please confirm whether you can provide above data ?
Best Regards,
Machida
Hello Machida,
We do not have the thermal numbers for the OPA134 and OPA2134 op amps. They were designed and characterized a couple of decades ago. I suspect their thermal performance was determined to be safe over their specified operating temperature range and when operated under normal conditions.
We might be able to provide you with some approximations of Rθja, Ψjt and Ψjb based on similar products, if they are available in the same package. Which package type were you planning on using?
Regards, Thomas
Precision Amplifiers Applications Engineering
Hello Ryuuichi,
A request has been submitted to have the thermal parameters for the OPA134 and OPA2134 SOIC package devices determined. As soon as we receive the information from Packaging Engineering I will post it here for you. I expect we will have it within a week.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas-san,
Thank you for your reply and response.
>A request has been submitted to have the thermal parameters for the OPA134 and OPA2134 SOIC package devices determined.
Thank you for correcting me. You are correct. I mistook package type.(I wanted to request SOIC not SO (OPAx134 do not have this package.))
Please keep watch on progress.
Best Regards,
Machida
Machida-san,
The thermal information for the OPA134UA and OPA2134UA devices has been derived by our Packaging Engineering team. Here are the results:
OPA134UA OPA2134UA
RθJA Junction-to-ambient thermal resistance 112.9 °C/W 106.9 °C/W
RθJC(top) Junction-to-case(top) thermal resistance 52.4 °C/W 48.1 °C/W
RθJB Junction-to-board thermal resistance 57.1 °C/W 50.8 °C/W
ψJT Junction-to-top characterization parameter 10.9 °C/W 8.0 °C/W
ψJB Junction-to-board characterization parameter 56.3 °C/W 50.0 °C/W
Regards, Thomas
Precision Amplifiers Applications Engineering