This is Dilip from HCL India, We are in need of one urgent information from your end. We are using Part number LMC7101. The datasheet from TI has the application circuit. It shows the inverting amplifier circuit, but specifies as non-inverting circuit(see below). Can you please check and tell if this is a typo error or this will be the intended application of this part. If this is the intended application what will be the output in open loop. In our application circuit if the input is an AC signal with ~10mV offset & 30mV amplitude (275Hz) what will be the output (only RA_Buf) will be active. Can you check and tell me the details as soon as possible since it is a high priority.