This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, i'm working with a OPA197 outputting a sine wave centered in zero with 1.76Vp , ie, 1.250 Vrms. The amplifier is powered with +-3.3V and i was expecting to get something close to a maximum source current of a Irms= 46mA (65mA peak as stated in the datasheet) but it turns out if i put a load that forces a current higher than 30mA, the amplifier doesn't provide it and it starts to clip the wave. Am i missing something ? Thank you.
Hi Henrique,
The amplifier may be able to source 65mA, but not at full output swing. As you increase the output current, you effectively lose headroom in your output voltage.The following figure depicts this behavior:
A 1.76V output signal puts you 1.54V away from the positive supply. If you look at the curve for 25C, you will notice that at (V+) - 1.54 you intersect the claw curve at approximately 30mA. The OPA197 can only source more current by limiting the output voltage, which is why you see clipping. The section where the curve drops off represents the short circuit current of the device.
Regards,
Zak Kaye