Part Number: THS4521
Other Parts Discussed in Thread: OPA2810, LMV794, THS4552, OPA354, TL7660, OPA837, TINA-TI
I am in the process of designing (Dual) Front End circuit with following specifications.
- Dual Front End circuit, with single power Supply with Dual –Ended inputs to OP-AMP
- Power Supply 3.3V
- Vin = +/- 2V
- Vout = 0 to 3V
- Voltage Ref. 0-3V output
- Low noise – Differential input to ADC
- Able to block AC signal – AC Filter 60Hz
- 10M Impedance
I am primarily looking for suggestions and recommendations if the part will work for the design consideration or if there are alternative parts and solutions.