This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi Zak,
thank you for your support!
for your questions, pls help comment besides the ref, anything need be changed, tks a lot!
1) What is the common-mode input voltage and differential input voltage range?
common-mode input voltage---48V,differential input voltage range----several 10s mV.
but as you can see from the circuit, the input is AC coupled, why should we concern about the VCM?
2) What is the gain?
26db.
3) What load is the INA128 driving?
phantom MIC.
Hi Vera,
In the configuration you have described, you cannot operate the INA128 with a 0V common-mode input (see plot below).
If you want to maximize your output swing and maintain linear operation then you will need to lift your input common-mode up to at least 4.3V. In this case the easiest solution would be to tie the same 6V reference to each of the 330kOhm resistors on the input.