This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
1.I am trying to design an power amplifier using OPA548 and 2N3055/MJ2955 transistors. But when I add capacitor of 100nF and 10 ohm resistor (in series) at the output, am getting distortion in the output signal. This experiment was carried out without any load. The images are in the attached file. I am unable to find the reason.
2. Upon connecting a induction motor at the load, If I suddenly change the amplitude of the signal (from around 7V to 30V), the PNP transistor is failing. I am unable to explain this phenomenon.capacitor.pdf
Hello P SUBRAHMANYA,
If you are driving the bases of the two output transistors with the OPA548, then adding the series RC network may be introducing a loop stability issue. When the output transistors are not driving a load their junction capacitances are likely different than when they are driving a high current load. Is there a reason you are adding the power transistors after the OPA548?
Please provide information about your OPA548 applications circuit. We need to see the circuit schematic, power supply information, input signal characteristics, detailed output load information and output signal expectations.
Regards, Thomas
Precision Amplifiers Applications Engineering