Other Parts Discussed in Thread: VCA820, , LMH6502, LMH6503
Hi
On the datasheet, it is defined as the below.
And,
The maximum operating voltage is not defined. However, VCA820 it is defined as +/-6V on the datasheet,
Can we refer VCA820 specs to as the max voltage of VCA822?
And I have one more question about operating voltage.
Can we use thie device with V=+5V and V-=GND(0V) condition? As the above specification we should use this device with V+=7V~12V if V- is GND.
Is my understanding correct?
Regards,
Koji Hamamoto