Other Parts Discussed in Thread: OPA363
Hi,
I'm using an OPA341UA under the following conditions:
Power: V+ = 5V, V- = 0V. Decoupled with 100nF
Output driving a NPN base through 100R.
SD pin: 0V or 3.3V (data sheet says thresholds are 0.8V and 2V) from microcontroller.
SD signal is on 250us every 25ms, or 1% duty.
But at times the SD os off for an extended period, e.g. several minutes. When this occurs the opamp does not come back to life. It just stays in shutdown and I have to cycle the 5V power to get it to come back.
Any ideas what may be causing the opamp to stop responding?
I've tried all sorts of decoupling on various pins...
Is it possible 3.3V is not enough for the SD pin (even though the data sheet shows 2V threshold)?
I'm stumped! Any help appreciated.
PS; for now I have made a work-around by powering the opamp off for 5ms every 25ms during a time when it's not needed, but I don't really like this solution!
Thanks, Ken