This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1200: AMC1200: correct wires for isolated vdd1

Part Number: AMC1200

Hi to all!.

I need to measure a variable voltage (0V -> 600V  range) with AMC1200.

I use a fully isolated dc/dc converter for build a 5Vdc for Vdd1-Gnd1.

For correct measurament i need to connect Gnd1 to return of high voltage, or can I leave it unplugged? (sse image)

Best regard, luca