Other Parts Discussed in Thread: LMH6321
Hi Sir/Madam,
I have a problem when using LMH 6321 as a standalone voltage buffer, as in the below figure shows, what I want to do is extracting a voltage signal from a electrical oscillator (which oscillates at 5 MHz) and then filter the DC component and finally drive another load oscillator. Since I do not want the load and the DC block to affect my electrical oscillator (which is the source), so I hope to use LMH6321 to realize unidirectional signal transfer.
But now I have problem: every time when I apply power to the LMH6321 (V+ and V-) before i turn on the electrical oscillator, I can see parasitic oscillation (~14 MHz) for both the output of electrical oscillator and the output of the DC block. When I turn on the electrical oscillator, the intrinsic output of the electrical oscillator and the output of the DC block all deformed and become noisy.
I do not know the output impedance of the electrical oscillator and meanwhile it has to be changed for our using. But I know the DC block and the load almost have 50 ohm input impedance.
since i do not have much eletrical background, I appreciate if anybody can help me to solve this problem.
best
Ke Huang