Hi team,
I have a question for 5.1. TI Precision Labs - Op Amps: Bandwidth 1. In this video, the input signal frequency is 200kHZ, the closed gain
is set to 100V/V. The GBW for OPA827 is 22MHZ. So, 200kHZ*100V/V=20MHZ<22MHZ, So, the 200KHZ input signal can be
normally amplified 100 times. That is when the input signal is 200KHZ, the closed gain should be 100V/V, correct?
But in TINA circuit, it shows the closed is 37.75dB when the input signal is 200KHZ. Would you explain this?