Part Number: OPA548
According to the OPA548 datasheet the device shutdowns at 160 degC and resets from shutdown once the junction returns to 140 degC.
I am driving a 8 ohm resistive load with a push pull configuration, at 8 V across the resistor to produce about 1 A.
See the schematic of one of the drivers:
At a heatsink temperature of about 70 degC, the voltage across the resistor drops momentarily and the E/S pin is pulled low momentarily. I will make a scope plot tomorrow, but it definitely drops out for less than a 100 msec.
I expected the junction to reach the thermal shutdown temperature, and then only after some **longer** time switch back on.
The TO-220 devices are mounted on a heatsink with a insulating thermal pad. I decreased the thermal resistance by changing the pads to Polycrylic Graphite Sheets, but the problem still occurred, only at a higher heatsink temperature (80 degC).
What I don't understand is how the device can shutdown and re-enable so quickly? Could this point to another problem?
Thanks,
Martin