I wish to make a PCB using Altium Designer.I am unable to find xtr111 in any of its libraries.Where can i find the library? Any ideas as to how i can create a PCB on Altium with xtr111.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Are there any other chips which are compatible in size and number of pins? i can use their foot print instead to make the PCB layout
Hello Juzer,
If you do not want to create your own footprint using Altium's built-in footprint creation wizard inside of the PCB libraries, then you can try to find another device that shares the same "MSOP-10 + POWERPAD" (DGQ) footprint. Some other product offerings from the Precision Analog team in the "MSOP-10+ POWERPAD" (DGQ) package include:
TLV4113
TLV2473
TLC083
TLC073
Hopefully Altium will have the footprints available for one of those models.
Regards,
Collin Wells
Precision Analog
Linear Applications
Thanks Colin. I noticed the XTR111AIDRCT being used on the XTR111EVM and hence chose to order those samples but i dont understand the difference or on what basis do i choose between DRC & DGQ .
Does TI provide the gerber files for the XTR111EVM?
Hi Juzer,
The XTR111 comes in two different packages to give customers a choice between a no-lead package (DRC) and a leaded package (DGQ). The DRC package is smaller (3mm x 3mm) due to the fact that it is a lead-less package and therefore will save some board space in the final application. The DGQ package is slightly larger (3mm x 5mm) but is easier to handle and assemble with because of the leads.
I will try to locate the GERBER files for the XTR111 EVM and post them on this thread.
Regards,
Collin Wells
Linear Applications
Hi Francisco Moya !
I really want to have the footprint with the altium designer of XTR111 , could you give me ? my email address : nguyenhuuson1989@gmail.com
thanks you so much , hope as soon as you can .
Regards !
Son!