Other Parts Discussed in Thread: TLV9064, TLV9002, TLV9061, TLV6741, LMV321
Dear Sir:
May I to know the release date of LMV321A? Thanks
Best Regard
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jason,
Thanks for your interest in our part. This device is scheduled for release early October.
In the meantime, can I interest you in the attached parts with similar performance and specs.
Device | lmv321a | tlv9064 | tlv9002 | tlv9061 | tlv6741 |
Num Channels | 1 | 4 | 2 | 1 | 1 |
VCC min (V) | 2.5 | 1.8 | 1.8 | 1.8 | 2.25 |
VCC max (V) | 5.5 | 5.5 | 5.5 | 5.5 | 5.5 |
Iq 25C max (mA) | 0.15 | 0.8 | 0.075 | 0.8 | 1.1 |
GBW/BW (MHz) | 1 | 10 | 1 | 10 | 10 |
Slew Rate (V/us) | 1.7 | 5 | 2 | 5 | 4.75 |
Vnoise (nV/√Hz) | 33 | 11 | 27 | 11 | 3.7 |
RR In | No | R-R | R-R | R-R | |
RR Out | R-R | R-R | R-R | R-R | R-R |
Ibias (typ) (nA) | 0.01 | 0.0005 | 0.005 | 0.0005 | 0.01 |
Vos (Max) (mV) | 5 | 2 | 2 | 2 | 1 |
Vos Drift (uV/C) | 1 | 2 | 0.6 | 2 | 0.35 |
Thanks.
Regards,
-Mamadou
Dear Sir:
Sorry for reply late. We used LMV321A for general voltage amplifier on IoT application. Our customer also used LMV321 but they don't need high voltage supply for OP. Then Supply voltage of LMV321A is 5V. It more suitable for our application. BTW , You mentioned above OP table , It have low ib suitable sensor application? right?
Best Regard
Jason