This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear sir,
Does TI have a rail-to-rail OPAMP (In or In to V+) that pinout the same as LM321?
Please refer below figure. DBV 5-pin SOT-23
And it need to operate under 12V supply.
Does TI have this solution?? Thank you very much.
CK Ho,
TLV2370, OPA743 and OPA191 are few options with high voltage (>12V) supply capability, comparable specs and RRIO. But these are not directly P2P compatible with LM321. You will have to swap your Pin1, Pin3 and Pin 4.
Lets us know if this is a viable solution.
Regard,
Sanjeev