Other Parts Discussed in Thread: ADS54J69, , LMH6881
Hello,
The question I have is if the 2 independent channels of the LMH2832 can be used, cascaded (The Output of Input A driving the Input of Input B) with the outputs driving a LMH6881 before ultimately driving an ADC (ADS54J69). The design would be 2 independent Signal channels in relative close proximity (about 2 inches apart on the same PCB) with each channel using this cascade approach as opposed to the two signal channels going through the 2 (two) LMH2832 ICs as Channel A and Channel B respectively. Each channel would have identical hardware and independent control and emerge at the 2 Channel ADC. I am wondering about any potential issues with this approach. Is it too much gain for a channel in such a small space going from A into B? The desired signal level range is relatively wide and the overall system gain is to be spread out into various sections. In a worse case the LMH2832 could either be applying maximum attenuation or maximum gain.
The maximum gain applied for 2 cascaded channels is my concern in this arrangement. Is this a common configuration for the LMH2832? I understand that the gain and attenuation can be finitely controlled and limited via the SPI bus however if software or firmware has the option to set the above scenario, are there ramification to the signal integrity (harmonics or compression, etc)? The data sheet typically shows the channels being used independently and in parallel. Has the LMH2832 or other similar devices been used successfully in this configuration and if so are there any guidelines? Thank you