Other Parts Discussed in Thread: INA190EVM, , INA190
Hello,
I just began to use theINA210 using the configuration of the INA190EVM. I have a questions to confirm that everything is set correctly.
1.I create a new combination for the INA 210 according to the schematic INA210
With he same values as in your EVM but i need to calculate the R81 value. The voltage for the unit is 14V the current to measure is 0.03 mA to .100mA. we want to measure something for .100mA should be something like 4 volts with a steps of 100mV for less current. if this possible. I assume also the power up for INA210 should be 5V, is that correct.
thanks in advance
Silvia.