This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In the datasheet of the AMC1200B I can see that the creepage as well as the clearance for the DWV package is 8mm (7.3.4).
In the AMC1301 datasheet I read a creepage of 9mm for the same package (7.6).
As of my understanding creepage and clearance is only defined by the geometry.
Any clarification is highly appreciated.
Thanks and best regards,
Patrick