This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA735: Input resistance of OPA735 is not given datasheet of IC

Part Number: OPA735
Other Parts Discussed in Thread: OPA335

Hi,

I am using opa735 in my application. I need the value of its input resistance but it is not given in the datasheet of IC. Can you tell me its value?

  • Hi Onkar,

    you can estimate it from the input leakage current. The input resistance is in the 10GOhm range at room temperature.

    Kai
  • Adding to Kai's answer, the input common-mode resistance may be calculated from the slope of the IB vs Vcm graph: Rcm=ΔVcm/ΔIB.

    Unfortunately, the graph is not shown in the OPA735 datasheet; however, you may see the trend in another zero-drift product datasheet, OPA335, shown below. From the graph below one may calculate the Rcm to be between ~100G (1E+11) at 25C to Rcm=~3V/150pA=2G (2E+9) at 125C.