This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
one of my customer using LM358AP (Dual Opamp) in their Fire alarm System .
Earlier they are using ST LM358N that we replaced by LM358AP .Now out of both OPamp (LM358AP) second Opamp do not operate.
Please check below observation tables of both devices.
LM358AP (TI) |
LM3358N(ST) |
|||||
Pins |
V at Non operating |
V at Operating condition |
Pins |
V at Non operating |
V at Operating condition |
|
IN1- |
21.8 |
17 |
IN1- |
21.8 |
18 |
|
IN1+ |
20.4 |
20.1 |
IN1+ |
20.3 |
20.1 |
|
OUT1 |
|
Working |
OUT1 |
|
Working |
|
IN2- |
22.5 |
22.5 |
IN2- |
22.5 |
22.5 |
|
IN2+ |
21.9 |
22.5 |
IN2+ |
21.8 |
22.5 |
|
OUT2 |
|
Not working |
OUT2 |
|
Working |
Please advise how we can resolve .
Hi Ronald ,
I mean to working and not working to Getting O/P from Out1 pin of Opamp and not getting O/P from Out2 pin of pin respectively .
Supply Voltage is 24V.
Sorry i didn't understand your answer .
My issue is when we are using TI opamp ,we did not get any output at OUT2 pin of Opamp .
And In the same board if we just replace TI OPamp by ST opamp we get output at OUT2 pin .
Please advise.
Thanks
Regards
Rahul
Rahul,
The LM358 does not have the ability to make the output high impedance therefore the output is always on.
The output may be incorrect due to the input common mode range.
With a 24V supply and full temperature range, the maximum input voltage is 22V (24V-2V). Your table shows 22.5V which is close to the edge.
Can you reduce the input voltage to 24V supply minimum - 2V?