This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2474: SMT Reflow Max Temperature

Part Number: TLV2474

Dear Amplifier team. 

Could you please get information SMT reflow max temperature of TLV2474AQDRG4Q1?

Thanks

Best Regards

Gerald

  • Former Member
    0 Former Member

    Hi Gerald,

    The short answer to your question is 260°C.

    This information can be found in the "Quality and Packaging" Tab of the device folder on ti.com (see attached image).  Under your part number, go to the "MSL Rating / Peak Reflow" column.  The "260C" means your part will have a max reflow temperature of 260°C.

    There's another great thread on e2e with several resources on this topic if you are interested in more information.

    Regards,

    Daniel