This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello user3830479,
To replace the AD8667, check our OPA2187. OPA2187 is a Zero-Drift(check out the tech note here: http://www.ti.com/lit/an/sbot037a/sbot037a.pdf ) wide supply CMOS OpAmp that easily goes head to head with the competitive device and dominates in all areas. Please see the spec comparison below and feel free to order some free samples from ti.com/product/OPA2187
Best regards,
Raphael Puzio
Specifications |
TI LMC6082 |
AD8667 |
Supply Voltage (V) |
4.5 < Vs < 15.5 |
5 < Vs < 16 |
GBW (MHz) (Typ) |
1.3 |
0.52 |
Slew Rate (V/µs) (Typ) |
1.5 |
0.26 |
Input Offset (mV) (Typ, Max) |
0.15 , 0.35 |
0.03, 0.175 |
Input Offset Drift (µV/°C) (Typ, Max) |
1, - |
1.5, 5 |
Input Bias Current (nA) (Typ) |
0.00001 |
0.0003 |
Noise @ 1kHz (nV/rtHz) (Typ) |
22 |
23 |
Iq per Channel (mA) (Typ, Max) |
0.45, 0.75 |
0.21, 0.275 |
Iout (mA) (Typ) |
21 |
7 |
Rail to Rail |
Out |
Out |
Operating Temperature (°C) |
-40 to 85 |
-40 to 125 |
Package |
SOIC-8, PDIP |
SOIC-8, MSOP |
Price (Web) |
$1.38 |
$1.58 |