Part Number: ISO122
Other Parts Discussed in Thread: ISO224,
Hi, Im using ISO122JU for analog signal isolation. Im isolating 0 to 3.3V with isolated power supplies . +VS1(15V) and -VS1(15V ground not negative voltage) and +VS2(iso 15V) and -VS2(iso 15V ground), and on applying 0 to 3.3V as Vin and its respective ground is tied to -VS1 or GND1 . Im not getting the same input as output . Im getting the output voltage around 12.8V on the output side of IC with respect to Iso 15V ground. Please suggest a solution for this problem.
Thanks
Naveen