Other Parts Discussed in Thread: LM293, TLV3401, LMC6772
Dear all:
The schematic diagram is as follows:
Question 1:Our products are all powered by a single power source (i.e., 5V, GND).Should the parameter "common mode input voltage" be considered in the LM293 comparator circuit?
Question 2:Because of the specification
Should the comparator input voltage meet this requirement (Vin+, Vin- less than 3V)?