Part Number: INA126
Dear Sir or Madam
I experience measurement errors occasionally, where it seems that the gain is too low. It helps to change INA126, but since there are 2 almost identical cycles and it is always the same that has the problem, I suspect there is something on the edge of the INA126 work area.
The only difference between the two circuits is the resistance from IN- (pin 2) to REF (pin 5). In the "good" circuit the resistor is 5k1Ohm and in the second it is approx. 10 times larger.
The input resistance of IN + is approx. 52k Ohm, RG is 1M Ohm, RL is 24k Ohm.
The circuits are used to measure on a PT100 sensor.
I have measured the gain to about 4.6 and it should be 5.08.
It is not always the fault that shows right away, so it may take several days for it to show up, which makes it more difficult to find.
Hopefully someone in here can point me in the right direction for my investigation.