Other Parts Discussed in Thread: TLV7031, TLV7081
I am making a circuit using the TLV3691 nano-power comparator using VCC = 3.3V. I want to connect one of the inputs directly to VCC. The other input is connected trough a 2 MEG resistor.
The 2 MEG resistor should prevent any damage to the part if the second input exceeds VCC.
But is there any performance degradation in input bias current, propagation delay, or input offset voltage when operating the inputs right at VCC?