This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello ACGUY,
Even if the bus voltage monitor functionality is not being used, the VBUS pin should be connected to a valid input voltage to prevent device damage. Any voltage from 0V to 36V will work.
Best regards,
Ian Williams
Applications Manager
Current & Magnetic Sensing