Dear Sir/Madam,
May I know what is the differences between these 2 body marking?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kum,
For small packages, where there is not a lot of room, both alphanumeric and binary "dash" codes are used.
"T1IS" which is one of the designations for the TL331IDBV.
The dashes above and below the text are a BCD binary code denoting the data and lot codes. The top row is the last digit of the year, and the bottom row is the month.
Both have a top code of "1000", or "8", or year 2018
The left has a code of "0001" (1, or January) and the right is "1010" (10, or October).
So the left is January 2018, and the right is October of 2018.